VBUS.DCOPERATION
Description
This parameter indicates whether the mains input is DC or AC.
If the mains input in DC and it is connected to DC+/DC- terminals (X3), not setting this parameter to 1 will cause “AC input phase loss” error.
-
- If using DC mains, Kollmorgen recommends that the mains input is connected to RST terminal as opposed to DC+/DC- terminal.
-
The reason is that the voltage of DC+/DC- may go above the mains voltage in regenerative breaking mode, and this can damage the DC power supply feeding the drive.
Examples
Usage
If the parameter is set to 0 ->1, the drive assumes that the mains input is DC, and phase loss detection as well as power loss detection are turned off.
If the parameter is set to 1 ->0, the drive assumes that the mains input is AC, and depending on the status of VBUS.THREEPHASE phase loss detection may be turned on.
Code
--> VBUS.DCOPERATION 0 --> DRV.FAULTS 1-2014: AC input phase loss. 2-2014: AC input phase loss.
--> VBUS.DCOPERATION 1 --> DRV.FAULTS No faults active
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 (ac mains) to 1 (dc mains) |
| Default Type | 0 (ac mains) |
| See Also | VBUS.THREEPHASE |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.